EATON.COM
Skip navigation elements to page contents
        Store Main Logo Deselected Cart Image
Cart
   Imagen del Pedido Deseleccionado
Orders
   Imagen de la Cuenta Deseleccionada
Profile
   Sign In Image
Login
   New User Registration
New User Registration
      
        eStore
 
 
STORE_BIN_TOP_LEFT_CNR_IMAGE STORE_BIN_TOP_RIGHT_CNR_IMAGE
Browse
Power Xpert
STORE_BIN_BTM_LEFT_CNR_IMAGE STORE_BIN_BTM_RIGHT_CNR_IMAGE

  

  Power Xpert STORE_CTLG_GRADIENT_IMAGE

 
PXM-4KUPG.jpg PXM-4KUPG - Power Xpert® Meter Upgrade PXM-4KUPG

Upgrade your Power Xpert® 4000 to a Power Xpert® 6000
Unleash the full potential of your power quality meter TODAY!


As one of the first power quality meter manufacturers in the world, Eaton is proud to offer a new and a unique feature for existing Power Xpert 4000 meter users: The ability to seamlessly upgrade to a more powerful feature set that has earlier been available only on the Power Xpert 6000 meters.

This new feature will allow you to use your existing Power Xpert 4000 just like it was actually a Power Xpert 6000 meter! All the features that you have learned to appreciate are still there, just like before, but now there will be all the additional features that you would normally enjoy only on a Power Xpert 6000 meter!

The upgrade includes a multitude of new features including the Events Timeline View. It allows you to plot color coded events on captured waveforms to gain insight into the sequence of events from one single cycle to the next one. This provides the user an excellent vantage point to review and compare multiple events at an unprecedented resolution.

For a full list of additional features gained with the upgrade please refer to the following feature chart.

Upgrade package contents
The upgrade consists of firmware upgrade license key that will be sent immediately to your designated email address upon purchase.
 
 
   
Purchase Price:     

STORE_CTLG_SKI_EDGE_IMAGE
  
STORE_BIN_TOP_LEFT_CNR_IMAGE
Welcome
Guest
Login

New User Registration

View Shopping Cart
No items

View Saved/Shared Carts

View Shopping Lists